8/7/2018 10:05 PM | |
Posts: 2 Rating:
|
Unable to install STARTER v5.1.1.2 on a user's PC running Windows 7. I have used this same installation media to install it on another PC running Windows 10 with no issues and the user has installed it on two other PC's (running Windows 7) with the media as well. It was initially installed on his PC but some components were missing, he uninstalled and now it refuses to install STARTER. I will attach the log file generated here, if you need any more info to troubleshoot let me know. EDIT: I have tried completely uninstalling all SIEMENS software from the machine using Revo Uninstaller, cleared temp files and any/all files left behind that contained anything related to Siemens. I have also updated the BIOS/firmware for the PC and Windows is up to date. Nothing is being blocked by A/V as we have the user white-listed. Tried re-installing and getting the same issue. AttachmentInstallStarterLog.txt (459 Downloads) |
Last edited by: dMilluh at: 8/7/2018 10:08:03 PMLast edited by: dMilluh at: 8/7/2018 10:08:31 PMLast edited by: dMilluh at: 8/7/2018 10:18:57 PM |
|
8/7/2018 10:18 PM | |
Posts: 2 Rating:
|
I've attached the current Windows version to this post. |
Follow us on