8/12/2018 10:25 AM | |
Joined: 7/24/2016 Last visit: 4/10/2025 Posts: 15 Rating:
|
Hi , I am using S7 5.6 software for plc and STARTER 4.5 for VFD .While working on S7 plc hardware config ,i can able to add a Micro master VFD and given a DP address successfully .after that i compiled and done the logic for VFD ON/OFF as well . But In the S7 project tree(down to CPU ) The same VFD is not visible . Can anybody help me for the procedure to add the same VFD on the project tree . Regards, Santosh Patro ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/13/2018 8:21:11 AMNew subject after splitting Last edited by: Jen_Moderator at: 8/13/2018 8:22:50 AM |
|
Follow us on