8/8/2018 7:48 PM | |
Joined: 3/23/2017 Last visit: 6/6/2025 Posts: 19 Rating:
|
Is drive rating ( converter rating R072:001 ) is nameplate rating or (1v=100% i.e. i/c ct ratio/baurdon resistance eg ct ratio 1000 & rp=0.909 ohm ,,,1v=>1100 amps=>convertor rating=>r72.001) & say motor rating is 500 amps, means p76:001==> apx 50%, then what should be op at x175 12-13 for motor current say 300 amps is it : 300/500*10 v ??? (is it for 300 amps ct op apx 300/1000=0.3 amp=>0.3*.909 v=>0.2727v acros burdon=> according to r72:001=> 0.2727*1100=>299 amps is op at x175 :12-13 is=>299/1100*10 or 299/500*10) is it correct ??? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/9/2018 6:25:30 AMNew subject after splitting |
|
8/13/2018 5:17 PM | |
Joined: 3/23/2017 Last visit: 6/6/2025 Posts: 19 Rating:
|
Thanks i will check !!! |
Follow us on