1/7/2019 10:26 AM | |
Joined: 2/18/2010 Last visit: 9/12/2025 Posts: 3 Rating:
|
Hi guys I have the same kind of problem : MLFB 6se7041 VC with K80 option , master and slave 750KW each , 400 vac and 1.1MW induction motor with 2 separate windings I have : and the fault condition (stored in r949) is sometimes 0 and sometimes 2 In such a case , Is the r949 contents significant or not ? Please could you help me ? Regards .. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/7/2019 2:31:21 PMNew subject after splitting |
|
Follow us on