(0)| 1/27/2019 6:50 PM | |
|
Posts: 4 Rating:
|
Hi there , I work for a cable Manufacturer. At Winding and twisting section of the cable we have two 6RA70 drives which drives two distincts motors each other. a)the first drive is in Speed Mode Master b)the second drive is in Torque Mode Mode Without Load when we start here is the reaction: a) the drive in speed mode reaach the speed at 100% as it displays on the drive b)The second drive in Torque Mode reach 75% as it displays on the drive. As the second drive does not reach 100% in torque the winding system does not work at all. We compare the parameters with another section winding and they are the same . Can Someone help on that / ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/28/2019 2:15:16 PMNew subject after splitting |
|
Follow us on