(0)| 2/8/2019 9:14 PM | |
|
Posts: 1 Rating:
|
FIELD OVER CURRENT ISSUE 6RA70 95 4GV62, 600V 2000A Field rating output - 375 v 40A Equipment 1000 HP Crane Hoist Motor. field = 5.4 ohms, rated field 38.5 amps ISSUE - field is going what looks like full on at 48 amps / Blowing 50 amp field fuses replaced - field control card, field rectifier and SCR module, cud card, firing control card, Par 102 set to 38.5 amps no changes made to system for the last 10 Months ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/11/2019 10:49:07 AMNew subject after splitting |
|
Follow us on