(0)| 2/22/2019 12:22 PM | |
|
Joined: 1/24/2009 Last visit: 6/19/2025 Posts: 85 Rating:
|
Hello, regarding SIMATIC 545 i face the following problem : When i power supply the system : The red led " CPU GOOD " is off The red leds " BATT GOOD " and " RUN " are on The red led " DC POWER GOOD " on the 505-6660 power supply module is OFF. Many red leds on the IO modules are on. CPU can't comminicate with HMI neither with pc to download a new program. I replaced the cpu, but same results. I replaced the 1st module ( POWER SUPPLY 505-6660 ) but same results. I pluged out all IO modules, even CPU but the POWER SUPPLY does not light the red led "DC POWER GOOD" Should i replace the rack too ? May be it is humidity problem inside the rack ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/25/2019 8:22:19 AMNew subject after splitting |
|
Follow us on