(0)| 9/30/2008 2:04 PM | |
|
Posts: 487 Rating:
|
PLCSIM has a menu option to change MPI address. Make sure MPI address of PLCSIM is what WinCC Flex is looking for. Also make sure Set PG/PC interface is set for MPI (5611, 5612 or PC Adaptor). I think it works only if you configure communication via MPI. The FAQ below is for protool but since the technique is the same, it may be helpful. http://support.automation.siemens.com/WW/view/en/13283804 |
Follow us on