10/14/2008 12:10 PM | |
Posts: 29 Rating:
|
Hello, take a look at this link, it is the manual of the inverter: http://support.automation.siemens.com/WW/view/en/23658214 There is a description of the alarm message A022in chapter 14.2. Perhaps this can help you. Regards |
10/15/2008 5:36 AM | |
Joined: 12/22/2007 Last visit: 4/10/2025 Posts: 52 Rating:
|
Thanks ...Stoppacher |
10/15/2008 9:06 AM | |
Posts: 29 Rating:
|
No problem. Regards |
10/16/2008 2:24 PM | |
Posts: 29 Rating:
|
Hello, Which alarm or failure messages do you have at the inverter at all? In the compendium there is P380 and P381. These are function parameters for entering the temperature threshold at which the alarm or fault massage istripped. Her is the link to the compendium: http://support.automation.siemens.com/WW/view/en/13472409 Perhaps this can help you. Regards |
10/17/2008 6:57 AM | |
Joined: 12/22/2007 Last visit: 4/10/2025 Posts: 52 Rating:
|
we already check parameter P380 and P381 =0.which parameter setpoint inverter temperature.we need your help.thanks |
10/17/2008 1:57 PM | |
Posts: 29 Rating:
|
Hello, sorry, there is nothing more occurs to me at the moment. The experts perhaps can help you along there better or you open a support request. Sorry Here is the information: For more technical consulting please contact the Technical Support for Automation & Drives SIEMENS AG Tel: +49 (0) 180 5050 222 Fax: +49 (0) 180 5050 223 Mail: adsupport@siemens.com Support Request: http://www.siemens.com/automation/support-request Internet: http://www.siemens.com/automation/service&support FAQ : http://www.siemens.com/automation/csi_en/product |
Follow us on