(0)| 10/29/2019 6:16 AM | |
|
Posts: 1 Rating:
|
Hi, I am using servo motor 1FK7063-2AF71-1RA2 with M0=11 Nm & Mn= 7.3 Nm while running I found that I gives 7.3 Nm at starting of servo motor & when its direction of rotation changes. I doesn't found 11Nm torque utilization at any point, means not at starting of servo motor & not while running. Where as If I give tool pressure of 20 bar (Hydrallic) motor stops working & gives contour monitoring alarm. Why. When I decrease pressure to 5 bar it motor works. I have to work with 20 bar pressure. Kindly guide me on this issue. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/29/2019 11:50:08New subject after splitting |
|
Follow us on