1/26/2020 2:51 PM | |
Joined: 3/27/2008 Last visit: 9/3/2025 Posts: 1212 Rating:
|
https://cache.industry.siemens.com/dl/files/400/24523400/att_33783/v1/420_OPI_24523400_en_1006.pdf See page 62 for the commissioning routine. This inverter drive is a Sinamics MM420, suitable for 400V, 3 phase operation. You also need a keypad. The spindle drive nameplate will have the necessary voltage / Frequency detail necessary for the correct operation. To operate the drive from the keypad set: P700 = 1. P1000 = 1 The drive will run from the keypad, stop/start and speed set point. |
Tractor |
|
1/27/2020 2:59 AM | |
Posts: 18 Rating:
|
am i forced to buy a keypad? |
1/27/2020 10:45 AM | |
Joined: 3/27/2008 Last visit: 9/3/2025 Posts: 1212 Rating:
|
This can be done via Profibus, I am not sure about the cost comparison however. |
Tractor |
|
Follow us on