(0)| 3/31/2020 5:35 PM | |
|
Joined: 10/1/2013 Last visit: 12/23/2025 Posts: 605 Rating:
|
Hi BOBILLIER, so far you've done everything right. Now what you need to know is that you can't use Technology objects for IO-Link reader. And TIA also won't show your PCT configuration. All you need to do is to configure the hardware (which you've done correct, I assume) and use some simple function blocks to communicate with the IO-Link module. You can find some example blocks here: |
| 4/1/2020 2:12 AM | |
|
Posts: 14 Rating:
|
Perhaps a start of solution with this post.here But how back to V3.0 library? |
Last edited by: BOBILLIER at: 04/01/2020 02:16:46 |
|
| 4/1/2020 4:14 PM | |
|
Posts: 14 Rating:
|
Hello Owei. I want make one remark about your previous proposition of Like i working with TIA V15.1 version and Library is in V14, i need automaticaly upgrade it when i install it in TIA. After installation, i have try to test LRfidOL_Read function. But when i compile them, i meet one error who said something like: " Invalid call because interface was modify since last time." and it's why i can't use this library. Any suggestion? Best regards Eric |
| 4/2/2020 11:25 AM | |
|
Joined: 10/1/2013 Last visit: 12/23/2025 Posts: 605 Rating:
|
Hi, attached you can find the updated library (V14 to V15.1). I called all the blocks in my program and compiled without errors. Edit: You can't use the integrated ident blocks from TIA Portal for IO-Link readers. You have to use the attached blocks or create them by your own :) AttachmentLRfidIOL_V15.1.zip (1014 Downloads) |
Last edited by: Owei at: 04/02/2020 11:27:45 |
|
Follow us on