5/25/2020 11:49 AM | |
Posts: 11 Rating:
|
Thanks for the answer. I checked the bus adress in P918: it's ok (7), see file in attachment. I also checked the type of the CBP card from the parameters (r826.2: 2 so CBP2) so I think the GSD file is the same for the two drives. I am blocked. The machine has broken down for 2 weeks. I have provided you with the two parameter files for the two drives: the old and the new and the program for the PLC of the machine. Can you check why the PLC cannot recognize the drive? I need your help. Thank you so much. My Email: [snip]
Attachmentmchoura.zip (423 Downloads) |
Last edited by: Jen_Moderator at: 05/25/2020 13:20:42Removed E-Mail address, doesn't comply with forum terms. |
|
Follow us on