8/31/2020 2:06 AM | |
Joined: 6/7/2015 Last visit: 3/24/2025 Posts: 29 Rating:
|
Hi, I have exactly the same problem, so when Rack '0' is in STOP then I can't get online with Rack '1' even though it is running. I will also try the 'Select online CPU' option, I'm sure this will fix it. However the question I have is..,shouldn't this happen automatically ? For example , if this happened in the middle of the night, isn't the redundant system meant to 'fail over ', without somebody having to manually intervene ? But then I guess the program continues to execute in the other CPU anyway :) Cheers ! ------------------------------------------------------------------------------------------ |
Last edited by: DRG158A at: 08/31/2020 02:43:46Last edited by: Jen_Moderator at: 08/31/2020 12:45:12New subject after splitting |
|
Follow us on