1/17/2009 1:47 PM | |
Posts: 21 Rating:
|
HI ALL, CAN ANYBODY PLS SUGGEST ME DO I REALLY NEED SOFTWARE FOR F01 TECHNOLOGY CONTROLLER FOR THE DRIVE BACKUPS WHICH I M ATTACHING . PLS DO THE NEEDFUL. THNX. Attachmentspindle_slide_21_11_08.pdf (571 Downloads) |
1/19/2009 8:00 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Go online to the drive and look at : display parameter n978 .This parameter has: In your case if this option is enable n978=1 you don't need to make changes. The technology function remains enabled even after a software update and does not have to be entered again after new software has been loaded into the flash EPROM. If this is disable n978=0 you also don't need to make changes. (exept from future if you diecide to use this drive in other application or make upgrades in current) But if n978=2 you must order this PIN code immediately from Siemens office in, because after 500h you'll receive F063 and your drive will block. How to make order see in manuals: Compendium Motion Control (MC 1.66) (page 1089). Hope this help you! regards |
Follow us on