10/29/2020 5:53 AM | |
Joined: 4/12/2013 Last visit: 9/5/2023 Posts: 11 Rating:
|
[snip] if we use S7-1515 2pn controller as Profinet IO slave device, Is there any limitation for number of bytes which can be assigned as Input or Output for the S71515 controller( 6ES7515-2AM01-0AB0)? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/29/2020 06:09:46New subject after splitting. Division of question into separate topics. Last edited by: dkv2106 at: 10/29/2020 07:35:41 |
|
10/29/2020 8:22 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
I think dkv2106 is asking about the size of the I/O area that is available if the 1500 CPU is used as an I-Device. If so, the answer is 1440 Bytes and Entry ID:109478798 has more details on this. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on