7/12/2013 7:29 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Starter software is there -http://support.automation.siemens.com/WW/view/en/64374921 |
This contribution was helpful to
1 thankful Users |
7/12/2013 7:29 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, which ControlUnit do you have exactly? Do you need the USB Drivers for G120? This Drivers ar installed with STARTER SW. The actual Starter you can download here: http://support.automation.siemens.com/WW/view/en/26233208 Regards Christoph |
7/12/2013 8:07 PM | |
Posts: 621 Rating:
|
hello umncho and christophD thank you for the rsponse look the attached photocopy this control unit and power module sinamics drives software driver CD.to go online. and also i want operator guide controlunit bop system manual and parameter manual please link the adress. |
7/13/2013 8:26 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
You forgot to attach. Meanwhile you ca use search option here to find corresponding manual alone.
|
7/15/2013 4:21 AM | |
Posts: 621 Rating:
|
Hello Umencho yes and sorry i forgot to attach the file see this attached file i have marked there in sinamics data cable communication port and i have the data cable. so i want to that driver software is it avail mean please send the link address. Attachmentsinamics_1.zip (682 Downloads) |
Last edited by: ALGUDKAR RAO at: 7/15/2013 4:23 AM |
|
7/15/2013 3:59 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hi, the operator panel looks like BOP-2 manual: http://support.automation.siemens.com/DE/view/en/42185248 The Parameterlist for G120 you can find here: http://support.automation.siemens.com/DE/view/en/36426537/133300 Regards Christoph |
7/15/2013 5:27 PM | |
Posts: 621 Rating:
|
hello ChristophD thank you for the response i install the stater software latest version but i am trying to communicate USB cable. but its asking the driver not detecting. last one year back one of my senior collegue he is doing one conveyor application project that time i saw one small CD along with sinamics CU and powermodule.but we lost that backup and also iam trying to download from the net but not supporting |
7/15/2013 7:58 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Have you downloaded latest version from the link given by ChristophD?? Also have a look at following link given by UMENCHOin other thread http://support.automation.siemens.com/WW/view/en/68792063 According to it, you will be asked to driver installation as soon as you connect USB cable after installing software, then follow the instruction and driver will be installed, you can find it in PG/PC setting box with name S7USB Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/15/2013 7:59 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, this little CD should only be the documentation for the Drive, no Driver. When you connect the G120 with the USB cable to the PC is there any unknow device in the device Manager of your pc? Which control unit do you have exaclty (MLFB?) and which FW Version is on it? Is there a point S7USB under PG/PC Settings? her are helpfull links: http://support.automation.siemens.com/WW/view/en/58880678 http://support.automation.siemens.com/WW/view/en/67638802 Regards Christoph |
Last edited by: ChristophD at: 7/15/2013 8:05 PM |
|
Follow us on