7/13/2023 9:13 AM | |
Joined: 12/18/2014 Last visit: 9/7/2025 Posts: 35933 Rating:
|
Can you show us a wiring diagram of the connection between the transducer and the AM2 module? |
7/13/2023 11:29 AM | |
Posts: 8 Rating:
|
This is the generator program. It is rather pretty basic that's why I'm sending the program I used to test all the Analogs as well.
AttachmentBoth programs.zip (631 Downloads) |
7/13/2023 11:36 AM | |
Posts: 8 Rating:
|
I use LOGO! 8.1 &8.2 |
7/13/2023 12:01 PM | |
Posts: 8 Rating:
|
Yes. I tried multiple ways to see what how I can get the analog signal. So far each time I connected the CT to my PLC it would go 1000 and stay there as if it's a DC current. So far the AM2 inputs did bring it down to 200A but the thing is I don't have any load on the change over switch. 200A will show on the I1 input and on U1 1000. The CT is 4-20mA but I changed my amplifier to 4-20mA. Am I using the wrong CT? AttachmentMN1_6c08e432-00be-47bb-837e-c2e0a208bc0e_1024x1024.zip (551 Downloads) |
7/14/2023 6:52 AM | |
Posts: 8 Rating:
|
Had to do this early morning. I hope this answers some questions.
AttachmentElectrical plus photos.zip (599 Downloads) |
7/17/2023 5:41 AM | |
Posts: 8 Rating:
|
Hi Ela Sorry what is an Ace PLC? |
Follow us on