1/3/2015 5:11 AM | |
Posts: 30 Rating:
|
Hello, EDIT ON 26/09/2018 Hi, When you guys set up Remote PLC Gateway (2.1.Setup of remote PLC), be careful because that IP is the one you set in Ethernet Properties - TCP/IPv4. If you do in a wrong way, you couldn't connect to your remote devices (PLC, HMI, etc,...).Best Regards, AttachmentHow to setup Teamviewer VPN.pdf (7742 Downloads) |
Last edited by: MinhPhong29 at: 9/26/2018 10:43:37 AMLast edited by: MinhPhong29 at: 9/26/2018 10:43:58 AMLast edited by: MinhPhong29 at: 9/26/2018 10:54:37 AM |
|
This contribution was helpful to
6 thankful Users |
1/3/2015 9:47 AM | |
Posts: 30 Rating:
|
Hello ChristophD, I did step by step as the attachment. I have added route to the PLC on the PG, but I can't find accessible nodes. |
6/19/2015 9:20 AM | |
Joined: 8/11/2011 Last visit: 5/17/2025 Posts: 51 Rating:
|
Hi, I can ping the remote Laptop via VPN, Thanks. |
7/3/2018 2:00 PM | |
Joined: 4/28/2015 Last visit: 2/29/2024 Posts: 8 Rating:
|
Hi everybody. I make a new documentation. The connection was tested between Windows 7 (local device) vs. Windows 7 (remote device) and Windows 7 (Local Device) vs. Windows 10 (remote device). Note: Windows running with Professional Licences, don't work with Windows Home Version..
AttachmentGuia de conexão remota TeamViewer - TiaPortal_Rev2.pdf (2484 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on