11/25/2018 11:53 AM | |
Posts: 32 Rating:
|
So TIBI68; With TIA Portal, there is no solution if there is no dongle, i must have it!! Thanks. Best regards. |
11/27/2018 2:56 PM | |
Joined: 2/16/2017 Last visit: 10/17/2024 Posts: 9 Rating:
|
Hi HH21, I was able to migrate the project to TIA Portal 13 in the past. Maybe you can do the same?
|
This contribution was helpful to
1 thankful Users |
11/28/2018 11:54 AM | |
Posts: 32 Rating:
|
Dear Wojtek N; I have tried it, but the TIA portal doesn't recognise the s7p project file on the folder path, i think because i haven't the Simatic Manager installed. I have only an old PG with simatic manager, so it's not installed on the same PC. So, if you have done the migration to V13, Can you give me the file on TIA V13, it will be esay for me to migrate it? And if you have other solutions, please tell me. Thanks. Best regards.
|
11/28/2018 6:36 PM | |
Joined: 2/16/2017 Last visit: 10/17/2024 Posts: 9 Rating:
|
#dP sure, but there is really nothing I can do that anyone else can't. The process is super simple:
That is exactly what I did. Then from this new project I simply copied the blocks to my existing project. The only thing that you might stumble uppon is versions conflict for P_SEND library if you ever need to re-compile the blocks. In that case all you have to do is to open the library and change the version on the right from a dropdown list. AttachmentMbma340_V13.zip (1173 Downloads) |
Last edited by: Wojtek N. at: 11/28/2018 6:38:28 PM |
|
This contribution was helpful to
3 thankful Users |
11/29/2018 10:18 AM | |
Posts: 32 Rating:
|
Dear Wojtek N; For the steps of migration i haven't problem, only the file of TIBI68 which i have downloaded was only a library, so i couldn't do the migration for .S7l. I looked for a sloution to crate a project on simatic manager with this library to have a .s7P, and it's done. When i started the migration, in the end i have a message that the version of step 7 installed is not appropriated (Capture), but step 7 is installed with tia portal, so i don't know what the problem?
Thank you for the project published with TIA v13, i have done the migration, and it ask me to compile before, and i have done it, but i can acceed to the two functions MBMA340 and MBMAREQ because they are locked, it's normal? Capture 2. Thanks a lot. Best regards. AttachmentCaptures.zip (1096 Downloads) |
Follow us on