6/7/2011 4:32 PM | |
Joined: 8/27/2006 Last visit: 10/22/2024 Posts: 719 Rating:
|
Also Check This DocumentAttachment19701610_ProSave_e.pdf (919 Downloads) |
The more you know, The more you know that you don't know |
|
6/7/2011 4:33 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, You will have to try to perform an OS update with the option "Reset to factory settings" See this link: how do you do an operating system update (OS update) on operator panels? Here is a manual of MP377, http://support.automation.siemens.com/WW/view/en/26248558 Search for OS update You can use MAC Address. Best regards, Wizard |
3/17/2012 8:58 PM | |
Posts: 1 Rating:
|
thanks |
4/2/2012 5:38 PM | |||||
Posts: 378 Rating:
|
Dear
I had similar problem. I am sure your pannel hardware is not damaged. The message you have seen "No image found..." does not mean picture, It is disk file image. Your pannel Operating System had corrupted (failed). The OS for this pannel is Win CE. Here is the steps I had done and works fine for me: 1. First you need to have Win CE OS in disk image format like .iso ( if you dont have contact SIEMENS or google for it) 2. Format a flash disk in FAT system and copy the file to the flash disk by your PC. 3. Power off your pannel then connect the falsh disk and USB keyboard to the pannel 4. Power up your pannel then the pannel will boot up from flash disk and starts loading 5. Follow the instruction and setup the OS 6. After the setup finished remove your flash disk then restart again 7. Now everything should be OK and you need to upgrade firmware I hope this helps and let me know your progress |
||||
This contribution was helpful to
2 thankful Users |
9/25/2012 2:56 PM | |||||
Posts: 2 Rating:
|
Dear, I have also a defective MP377 (not booting) "Starting windows CE.. Please Wait.. I tried the steps, but the panel is not booting from compact flash card. 1) I have WIN CE.6.0 - ZWTiSO 2) I formated a flash disk in FAT system and copy the file to the flash disk by my PC (ISO format). 3) I conected my compact flash card to the MP377 4) Powerd up my panel, but it was not booting from the flash Do I need the Cab. & arm files? |
||||
9/25/2012 6:09 PM | |
Posts: 378 Rating:
|
Dear Elektron27, For WinCE 6.0 you need to burn ISO image to the flash disk. Try this tool : http://www.isotousb.com/isotousb_setup.exe and dont forget to enable USB booting on BIOS. Regards, |
5/10/2018 12:16 AM | |
Posts: 1 Rating:
|
Bro you just save my life...ty Put the device ip 10.100.3.2 -> set tcp/ip comunication Change wire connection from auto(dhcp) to 10.100.3.99 |
Follow us on