2/22/2024 6:43 PM | |
Posts: 24 Rating:
|
Hi, I have the same problem but with Software version 8.4. Today I have replaced my old OBA7 blocks with the new 8.4. Everything that is linked to the first block (master) works as expected. The checkbox "Allow S7 access" is checked. Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/23/2024 08:56:43New subject after splitting |
|
2/22/2024 6:47 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
Please upload your network project as a zip file to the forum. |
2/22/2024 7:21 PM | |
Posts: 24 Rating:
|
Hi, I have attached it here. Steve AttachmentLOGO84.20240222.snp.zip (539 Downloads) |
2/22/2024 7:30 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
I can't load your project in LSC V8.4. If I try then comes the message "Unknown error". |
2/22/2024 7:37 PM | |
Posts: 24 Rating:
|
Hm ok. I can open it on my Macbook in version 8.4.0. Maybe that's the issue? (Mac) Steve |
2/22/2024 7:53 PM | |
Posts: 24 Rating:
|
See in attachment. Thanks! AttachmentLOGO84.lsc.zip (624 Downloads) |
2/22/2024 8:05 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
Are you sure that you have added in the network project LOGO!8.4 slave devices? |
2/22/2024 8:16 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
Hmmm ... the lsc file can I open without problems. |
2/22/2024 8:18 PM | |
Posts: 24 Rating:
|
You can see the "Device type" is set to "LOGO! 8.4 Slave" when you open the properties of a Network Input. So that should be okay I guess. |
2/23/2024 4:28 AM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
I have rebuild your network project of the base of the lsc file that you upload. Try this. Have you set the real LOGO"s 8_2 (192.168.1.102) and 8_3 (192.168.1.101) into the slave mode? AttachmentLOGO84_2024_02_23.zip (400 Downloads) |
Follow us on