2/3/2025 9:21 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello Winchester7! In relation to what you mentioned, how is the PG/PC interface configured? I am attaching an entry that I hope will be useful for you in configuring it. https://support.industry.siemens.com/cs/es/en/view/89852595
Also, do you have SIMATIC NET installed? Finally, I am also adding an FAQ that I hope will be helpful. https://support.industry.siemens.com/cs/es/en/view/109803668 |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
2/12/2025 10:01 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello again Winchester! As bit7 mentioned, the first I would try then is to run the PLC simulation through PLCSim, to check if we can achieve the connection through this software. I would also try updating to the latest available version of v19, in this case, update 3, to work on the most developed and corrected version. - Updates for STEP 7 V19, S7-PLCSIM V19 and WinCC V19 Another thing that comes to mind is that you might be using the maximum CPU resources for it to communicate with an HMI. I am attaching the following FAQ so you can take a look and we can rule this out. |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
Follow us on