3/21/2012 11:23 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Hello, together we are working on this and try to reduce the "down"time of the forum. Best regards O_Moderator |
4/8/2012 9:51 AM | |
Posts: 8946 Rating:
|
This problem happens to me also very often. Since my start-up here in 2008, this is not an new problem. Many times, I send a message twice because of that. |
4/18/2012 7:59 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
OK I got it... It was adblock Plus... I got from solution from here Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
4/19/2012 2:37 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello , I experienced a really rare and strange phenomenon.While completing a post and uploading an attachment,I lost my log in status.It is rare but it is like a disaster to remember all sentences There is some complains in the German conference. Problem mit dem Forum: Login geht verlorenBest regards, Hamid Hosseini |
4/19/2012 2:55 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello, I also experienced a really rare and strange things, The Thanks & Rate Button in not dispaly for Some User Post, See the Screen Shot.... AttachmentSiemens.zip (668 Downloads) |
Ammy |
|
4/19/2012 3:06 PM | |||||
Joined: 10/3/2010 Last visit: 9/12/2025 Posts: 1568 Rating:
|
Sometimes this part:
is reduced to
|
||||
B r g d s , |
|||||
4/19/2012 3:30 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
After missing stars scenarion here,this is new in attachment. Missing stars,"thanks" and buttons all together. Best regards, Hamid Hosseini Attachmentmissing objects.zip (647 Downloads) |
4/19/2012 3:31 PM | |||||
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
This is old problem and mostly its because of heavy load And if you are using IE 7 or 8 then compability button always helps and For Mozilla, we dont have any option other than Type web address again in addressbar..And thats why I mostly prefer Open in New Tab button to see any forum so that I dont loose that FORUM button to go back to main page Regards Devesh Vithani |
||||
Last edited by: Vithani at: 4/19/2012 3:50 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|||||
4/20/2012 4:21 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Error in showing No of reply is still not fixed Have a look at attchment. When I tried to sort Micromaster Forum by No of Reply, I got first with -1 reply, which already replied by Umencho and second with No reply- which replied by Graeme I noticed same thing for this threads few days back too Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
4/23/2012 11:48 AM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
Hello Vithani, the refered post was published at the last day of the month. Actually the statistic for thread which got the last reply at the last day of a month isn't shown correct. The bugfix is allready available. But during campaign we want to avoid a deployment of the software. So maybe we could live with this feature one more month Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on