8/22/2022 3:43 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
Has every cylinder only one switch for the positions or two switches? |
8/22/2022 4:23 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
The magnetic sensors on the clamps by which position? Open? Or close? |
8/22/2022 4:26 PM | |
Joined: 8/22/2022 Last visit: 2/10/2025 Posts: 10 Rating:
|
clamps open will put the state closed. |
11/11/2022 9:53 AM | |
Joined: 8/22/2022 Last visit: 2/10/2025 Posts: 10 Rating:
|
Hi, The programme that I have written now repeats how I would like - I was wondering if anyone can help me with one last thing. I would like to use two inputs - stop button and reset into the programme. Stop - stops the cycle as it is. Reset - only reset once sequence has stopped and then energizes Q1 - Q2 - Q3. then once started the sequence carries on from Q4. I'm open to any improvements my programme needs. thank you in advance Attachmentsequence for laster cutter strpping bench.zip (733 Downloads) |
Follow us on