7/8/2013 8:47 PM | |
Posts: 23 Rating:
|
Ok i send the program it calls " wire magnetized" and already check the parameter r014 and it show the speed reference.. if you need more information here i am above the crane testing. waiting your responses. Regards Vithani. Attachmenthold cables magnetizados.zip (431 Downloads) |
7/8/2013 10:55 PM | |
Posts: 23 Rating:
|
TO: Vithani The brake open normally as soon as i start the drive. yes i will sent you the Program in PDF. any question do you have here i am. Regards. AttachmentParametros hold drive wire magnetized.zip (439 Downloads) |
Last edited by: arthr at: 7/8/2013 11:40 PM |
|
7/8/2013 11:58 PM | |
Posts: 23 Rating:
|
To: Vithani i already check the PMU when i set the drive with the parameter P443 to 58 and the PMU show 009, when i star the drive in the r014 display only ¨0000¨ and the motor turn slowly, i returd the parameter P443 to 507 , and i star the drive , the r014 display ¨44¨ with 1 volts in the analog speed referece in the control terminal strip X-102, and the same beaviour occurs. im waiting your answer. Regards Vithani.. i sent you the Program in PDF, the control brake is with PLC, this PLC AttachmentParametros hold drive wire magnetized.zip (441 Downloads) |
Follow us on