4/13/2021 2:13 AM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35928 Rating:
|
Hmm, strange behavior. Since I do not have the same hardware (no 6ED1055-1MB00-0BA2 expansion module) and neither do I have your program, so it's difficult to make a statement. If Siemens doesn't provide any absolute information about what exactly was changed when the model changed from LOGO! 8.2 to LOGO! 8.3, no one except Siemens can make a clear statement. I would recommend to start a Support Request.
|