5/13/2021 3:42 PM | |
Posts: 14 Rating: (0) |
ok that's perfect ^^ but I have to make a program for the ktp a model like this kp300 is correct? |
Last edited by: Ameux at: 05/13/2021 15:48:39 |
|
5/13/2021 4:05 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
No, you do not have the same display as on the LOGO! Display or TD (E).
Yes, this HMI can you use with the LOGO!. |
5/13/2021 5:56 PM | |
Posts: 14 Rating: (0) |
Ok, to finish the best would be to upgrade to an oba 8 which |
5/13/2021 6:04 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
I think, that is the right way. If you buy a actually new LOGO! 8.3 then can you: - older LSC versions upgrading to LSC V8.3 for free. Download for LOGO! 8.3 Software UpgradeBut the download is export restricted. Why do you have to log in and register for downloading export-restricted software and what data do you need for this?In the company field enter "private use". |
Follow us on