2/16/2009 12:37 PM | |
Joined: 1/23/2009 Last visit: 7/20/2024 Posts: 29 Rating:
|
Hi, I got problem with INSYS GSM 4.2 LOGO!. I am working a long time with LOGO! and now I wanna use LOGO! with INSYS GSM modem. Everything is OK about LOGO! and INSYS GSM modem, AT command is OK, alarm input is OK, I send AT command via SMS to control INSYS outputs, INSYS send me SMS or PA SMS when something happened on LOGO! inputs or INSYS inputs. INSYS inputs and outputs work fine. LOGO! work fine with or without INSYS, but INSYS react only on changing LOGO! inputs. (P.S.LOGO! outputs and INSYS inputs are not connected) For monitoring of LOGO! digital inputs and outputs and flags I setup software parameter on the same way… My problem with INSYS is monitoring of LOGO! digital outputs (Q1, Q2,…), LOGO! digital flags (M1, M2,…), and also LOGO! analog outputs and analog flags. INSYS send me a SMS only for LOGO! inputs?
Thank you for replay ...I am a begginer with INSYS modems ... Best regards Dragan M. And here is my INSYS GSM 4.2. settings. AttachmentMonitoring I,Q,M,AI.zip (745 Downloads) |
Be creative while inventing ideas and be disciplined while implementing them... :) |
|
Follow us on