6/2/2021 2:24 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2151)
|
Hello ajpawar, You need to have installed and licensed the option WinCC/Audit. see manual "SIMATIC HMI WinCC V7.5 WinCC Information System" https://support.industry.siemens.com/cs/ww/en/view/109762744/115783869579
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
6/4/2021 8:46 AM | |
Joined: 4/6/2021 Last visit: 2/17/2022 Posts: 14 Rating: (0) |
Hi Georg, I've installed WinCC Audit and its license, now I can able to assign more than one user in esignature. In WinCC manual there is very small information about esignature. I'm still confused about option "Signature Required: Immediately/Retroactively" I've tried both options as shown in attached images. When I set it to "Immediately" then the button can be pressed only after signing of both Operator and Laboratory users, in this sequence of signing is not possible which is drawback. Is there any method to assign sequence of esignature? When I set it to Retroactively then the button can be pressed even after signing of either user, which should not happened because I've used AND logic operator. So what is the exact use of these options immediately/retroactively? Regards, Aman Pawar AttachmentImages.zip (165 Downloads) |
6/4/2021 10:17 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2151)
|
Hello ajpawar, I think, the answer is in the manual of WinCC/Audit V7.5 SP1 https://support.industry.siemens.com/cs/ww/en/view/109749101/114589047691 I have not the option WinCC/Audit availabe here, therefore
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on