6/4/2021 7:08 PM | |
Joined: 11/8/2017 Last visit: 9/7/2024 Posts: 335 Rating:
|
Hi, The Ring topology that's shown in the original post attachment shows 2 ethernet switches. I believe these are from the Siemens Scalance range. They are managed switches that provide the ability to operate the network in a Ring configuration, and provide a level of redundancy if a failure occurred in any single connection from device to device. There's a section of the forum HERE where the system is discussed. My knowledge on these switches is limited, but from what I understand, one of the switches would act as a Master, and the other as a Slave. There would be 2 physical routes that the Master uses to communicate with the Slave. The first/primary route is from Master > PX > PX > PX > Slave. The secondary route is from Master > Backup Route > Slave. The Master will decide which route to take to ensure that communication to all PXs in maintained. I would assume that information is provided via the Scalance UIs that detail where the ring-break failure has actually occurred. Regards, |
Last edited by: _CJ at: 06/04/2021 19:23:18 |
|
6/6/2021 4:34 PM | |
Joined: 8/27/2016 Last visit: 7/19/2024 Posts: 29 Rating:
|
Dear Expert Please send me document "CM110668en_01.pdf" David |
Follow us on