6/14/2021 11:19 AM | |
Joined: 5/4/2016 Last visit: 6/3/2024 Posts: 17 Rating:
|
During the engagement there are 3 mechanical positions, see pictures attached. I will have to make several posts, because only one attachment seems possible per post. Maybe the 3rd position is never reached in your case. For the combination available at my desk (SQV91P30 + VPF43.50F16) the automatic calibration works fine: position 3 is reached as soon as the stem is completely extended. When I do the manual engagement by turning the handwheel clockwise slowly and carefully, I can reach position 2. When I keep turning, there is a second click (See video attached) and position 3 is reached. Can you try, if it works when you use manual engagement? If it does not work, you could try to push down the spindle coupling by hand (See picture attached) when the stem is retracted completely. If the 3rd position is reached, but the disengagement still happens, we will have to check the spindle head dimensions. In order to do so, I am kindly asking you to open a Support Request. AttachmentPosition2to3manually.mov (746 Downloads) |
6/14/2021 11:19 AM | |
Joined: 5/4/2016 Last visit: 6/3/2024 Posts: 17 Rating:
|
|
6/14/2021 11:20 AM | |
Joined: 5/4/2016 Last visit: 6/3/2024 Posts: 17 Rating:
|
|
6/14/2021 11:20 AM | |
Joined: 5/4/2016 Last visit: 6/3/2024 Posts: 17 Rating:
|
|
6/14/2021 11:21 AM | |
Joined: 5/4/2016 Last visit: 6/3/2024 Posts: 17 Rating:
|
|
Follow us on