4/21/2015 9:12 AM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating: (7) |
Hello Tagolover, Is this also possible on TIA Portal (PC station to PLC communication via USB)? It seems the only option I'm seeing on the "Communication Modules" is Profinet/Ethernet, Profibus, and WinAC communication. Is there any other way it could work just as the WinCC? Thanks.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/21/2015 4:07:19 PMNew subject after splitting |
|
6/14/2016 11:26 AM | |
Posts: 46 Rating: (0) |
Hi all, communication between WinCC professional RT V13 & a S7-300 cpu(313c-2dp) over old pc mpi adapter (in mpi mode) is possible ------------------------------------------------------------------------------------------ |
Last edited by: projjwal at: 6/14/2016 11:27:48 AMLast edited by: The Helping Hand at: 6/14/2016 11:29:27 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
6/14/2016 1:51 PM | |
Joined: 8/21/2014 Last visit: 9/13/2024 Posts: 1035 Rating: (14) |
I'm sorry, I thougt that this was a new question and split up the thread. I moved your posts back to the original thread, now.
Sorry for the inconvinience. Best regards The Helping Hand
|
My Forum is the place to personalize your profile, |
|
Follow us on