10/16/2018 8:53 AM | |
Joined: 7/30/2012 Last visit: 5/12/2024 Posts: 335 Rating: (12) |
Hello, Is there any option to use G-Code interpolation in S7-1500T? is anyone using this GCode2MovePath tool |
10/17/2018 11:02 AM | |
Joined: 10/11/2006 Last visit: 5/17/2024 Posts: 5843 Rating: (793) |
Hello @KB@, With S7-1500 T you have the possibility to use the TO_Kinematics which enables you to solve different types of kinematics. One comfortable way to set the kinematic in motion is with the LKinCtrl – MovePath (FB), where you can program your linear and circular commands in a list called PathData (DataBlock). If you want to program G-Code you can use the GCode2MovePathTool to generate the PathData source automatically from the G-Code. Here you can find the documentation for detailed information – chapter 3.4: https://support.industry.siemens.com/cs/ww/en/view/109755891 |
Last edited by: Jen_Moderator at: 10/17/2018 1:06:59 PMOptimized link. With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on