8/18/2021 3:44 PM | |
Joined: 12/18/2014 Last visit: 6/16/2024 Posts: 33202 Rating: (4106)
|
The new functions of the LOGO! 8.3 is only available if you have a new LOGO! 8.3 buy. Older LOGO!s can't be upgraded to the new functions using a firmware update. There is no firmware update for it. And you need the current LOGO!Soft Comfort V8.3. If you already have a version of LSC, you can upgrade it to V8.3 free of charge. Here can you download the upgrade: Download for LOGO! 8.3 Software UpgradeBut the download is export restricted. Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
This contribution was helpful to2 thankful Users |
Follow us on