3/30/2021 3:19 PM | |
Posts: 39 Rating: (9) |
Hi, maybe you guys can help me with PXC5 network configuration for Modbus TCP gateway integration. I have gateway with 192.168.1.x IP and unit ID 23 (Like Modbus RTU address defined on the gateway). How can I define this device in ABT when there is no option for device address, just only setting for port number (default 502). Any ideas? Because with no address I receive that gateway is missing despite Modbus Poll and Modscan programs can receive all the date scanned from gateway without no problem. Maybe there are syntax for I/O configuration or something? I used Similar topic: PXC4.E16 modbus TCP problem - Entries - Forum - Industry Support - Siemens |
Last edited by: AutoGen_9341646 at: 03/30/2021 15:24:20Last edited by: AutoGen_9341646 at: 03/30/2021 15:41:41Last edited by: AutoGen_9341646 at: 04/01/2021 10:13:21 |
|
5/10/2021 3:01 PM | |
Posts: 39 Rating: (9) |
Any ideas? |
5/11/2021 12:23 AM | |
Joined: 7/25/2012 Last visit: 10/8/2024 Posts: 272 Rating: (84) |
NO, sorry, I don't know more, how to integrate this particular device |
Best regards, |
|
7/24/2021 7:15 AM | |
Joined: 8/13/2019 Last visit: 9/3/2024 Posts: 1 Rating: (0) |
helloAutoGen_9341646I have the same issue. now do you solve it? |
7/26/2021 7:12 AM | |
Posts: 39 Rating: (9) |
Hi, unfortunately no. I had to use RS485 instead of TCP...
|
This contribution was helpful to1 thankful Users |
Follow us on