9/24/2021 12:43 AM | |
Posts: 1 Rating:
|
Como me conecto a un s7-200 CN CPU 226CN?? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/24/2021 09:13:49New subject after splitting |
|
9/24/2021 12:37 PM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12407 Rating:
|
Hello Alonso; To connect to a S7-200CN CPU, there is an additional trick yhat you need to apply. The S7-200CN was a product developped by Sieemns and (originally) marketed only in the Asian market. The computer where Microwin 4.0 was installed (in English) needed regional settings set to China, or India, any country where the S7-200CN market was aimed at: •Open
the System Control panel of your PC •Open “Region and Language Settings” •Change
the setting of the location to one of the countries where S7-200CN is sold •Press
“OK” and close the system control panel •Now you should be able
to transfer programs from a S7-200 CN with Step 7 MicroWin 4.0 SP7 in English. The file in attachment was found on the forum a few years ago, but I can no longer locate the source, It is very clear and precise, so I would like to than the (now anonymus) poster who sent it. Hope ths helps, Daniel Chartier AttachmentProgram_a_S7200CN.zip (1015 Downloads) |
Last edited by: dchartier at: 09/24/2021 12:38:49Last edited by: dchartier at: 09/24/2021 13:10:54Last edited by: dchartier at: 09/24/2021 13:13:42 |
|
This contribution was helpful to
1 thankful Users |
Follow us on