10/5/2021 8:22 PM | |
Joined: 9/14/2018 Last visit: 2/29/2024 Posts: 1 Rating:
|
Hello, We have the same issue. We changed our server twice, with no success. Prior to the server replacement, Industrial databridge would disconnect (yellow indicator) and reconnect (green indicator) every 5 seconds. That would seem to have patched the bug. Now, everything works fine, except the connection to the IT SQL table, which only works 2 or 3 times, then the ADO component gives an error. Industrial databridge v7.01.5073a with WinCC v7.0 + SP2 + UPd3 Any ideas ? Edit : Turns out since we couldn't read, the insert we were doing right after on the row supposed to be read wasn't working. That's what caused the ADO error. But, we still can't figure out why we can't read after about an hour after starting up databridge. With the logs, I could get these errors: (TPEvtSQL) <--- FireTriggerEvent (0x80004005) (TPTrigger) <--- Evaluate (0x80004005). The rest of the log seems to be identical to the part which was working well. Also, it still confirms the connection to the IT SQL. Can someone explain these error codes to me ? Thanks, Gabriel ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2021 10:48:12New subject after splitting Last edited by: GChicoine at: 10/14/2021 13:37:31Last edited by: GChicoine at: 10/14/2021 13:39:59 |
|
Follow us on