10/6/2021 5:58 AM | |
Joined: 12/18/2014 Last visit: 8/30/2024 Posts: 33648 Rating: (4182)
|
Delivery release of LOGO! CIM (6ED1055-5MC08-0BA1)LOGO! CIM is an additional communications module for LOGO! 8.3 LOGO! CIM enables sending and receiving SMS and transferring data from LOGO! 8.3 basic devices to the AWS Cloud. With the integrated GNSS receiver (GPS), the position can be tracked and passed on. The built-in Modbus RTU interface supports Modbus RTU stations with RS232, RS485 und RS422 Interface. The most important functions for LOGO! CIMwithoutCellular Engine:
The most important functions for LOGO! CIMwithCellular Engine:
Important note: The following additional components are required for operation with Cellular Engine (not included in LOGO! CIM):
|
Follow us on