11/3/2021 11:21 PM | |
Posts: 257 Rating:
|
Hello SIOS Forum Community Firmware updates can be performed using a SIMATIC memory card. A firmware update can also be performed in one of the following ways: ●using the online and diagnostic tools of TIA STEP 7. ●using the standard "Module information" web page of the web server ●using the SIMATIC Automation Tool For more information, refer to the S7-1200 manual from page 137 in chapter 5.5.5 PLC Basics under the search term: Firmware Update. Note The procedure described in this article refers to the time of writing this article (status: November 2021). With kind regards SIMATIC International Technical Support Hub |
Follow us on