12/10/2021 6:26 PM | |
Joined: 2/17/2020 Last visit: 4/30/2024 Posts: 994 Rating: (169) |
Hiramrao, Please review these two requirements and configuration links to ensure that the SCADA architecture can work: What are the requirements for operating SIMATIC WinCC in a Windows network? Configuration of a Client–Server System with WinCC V7.5 Also, is the exact same version, including Updates, of WinCC RT installed on the client? |
A rating will be well appreciated. |
|
Follow us on