12/20/2021 2:52 PM | |
Joined: 11/2/2021 Last visit: 7/15/2025 Posts: 1 Rating:
|
Hello everyone, i have a problem with communication between HMI Siemens TP277 6" and PLC S7-200 with CP243-1 Ethernet module. These devices are connected via ethernet. My problem is with the panel hmi because every time after reboot, hmi comes back to transfer mode. More details in atachmend. HMI IP: 192.168.0.25 CP243-1: 192.168.0.22 PC: 192.168.0.44 Attachment123.zip (742 Downloads) |
12/20/2021 4:11 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Perhaps this link might help: Best regards, Wizard |
Follow us on