1/1/2022 7:03 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello pankaj_054, Which is controller? or project? If you had provided detail information, it would had been much better to help you. BTW, please refer below FAQs which may help you. How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible? How can you visualize the current status of the CPU on a WinCC flexible operator panel? How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Demo projects for SIMATIC Panels (WinCC flexible 2008), Panel PC and WinCC flexible PC Runtime WinCC flexible Getting Started Options MICROMASTER/SINAMICS G: Speed control of a G120/G120D/MM4 using a S7-300/400 (STEP 7 V5) with PROFINET/PROFIBUS and HMI |
Last edited by: PISCEAN 2010 at: 01/01/2022 07:04:50 |
|
This contribution was helpful to1 thankful Users |
Follow us on