12/23/2021 3:49 PM | |
Joined: 4/6/2021 Last visit: 3/21/2025 Posts: 2 Rating:
|
I have the following issue when I write a register from a TP1900 to a A8000 device:
The read external registers are shown on HMI correctly, without any problem. The communication protocol between the two devices is Modbus TCP/IP. Devices: HMI: TP1900 Comfort (SLAVE) A8000: CP8050 + CI8520 + CI8551 I did some tests:
Used my PC with the IP address of HMI, and wrote the same register from ModScan.
Used my PC with the IP address of HMI, and simulated. I cannot identify any difference between the two captures. Attached additional informations: Setting conection Defining external tag Defining internal tag The writing command on HMI
Wireshark captures AttachmentAdditional_info.pdf (371 Downloads) |
Follow us on