4/12/2018 9:33 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, perhaps this link might help: Why are fonts and objects shown shifted on a PC Runtime system or operator panel? best regards, Wizard |
This contribution was helpful to
2 thankful Users |
4/16/2018 3:26 PM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello Impala6107 We have made many tests with the different DPI Settings in order to work with comfort Panels and it es very important if you get a Project from another Computer (with different DPI Settings) or if you do changes in your DPI Settings in the Windows you have to do a recompile all, that the Whole Project is generated in the correct DPI Setting. -> https://support.industry.siemens.com/cs/ww/en/view/13899072 (As Wizard already posted"!! This works on all our Systems also with TIA V15. Try also: - Make a backup of your Project - Close TIA Portal - Delete "IM" Folder in the Project Path - Reopen TIA Project and do a recompile all If it still doesn´t work please send Screenshots that we can "see" your problems. Bye Murof |
Last edited by: Murof at: 4/16/2018 3:27:22 PMLast edited by: Murof at: 4/16/2018 3:28:00 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
1/21/2022 10:21 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Hi Users, I have forwarded the topics regarding 4K resolution to the responsible person and got the following answer
Best regards, |
Follow us on