2/2/2022 9:56 AM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16322 Rating:
|
Hello In the first example you use the wrong Screen Path. If you use an absolute access to the screen you have to use the Screen context path. its discribed in the Help System: https://support.industry.siemens.com/cs/ww/en/view/109794202/36126590859 (Its because you can open the same screen multible times in different screen windows...) Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/2/2022 10:06 AM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16322 Rating:
|
An the second example: Should work Work with Trace diagnostic outputs to see if the script does not run or where is the problem. Here are some basic information: https://support.industry.siemens.com/cs/ww/en/view/24074628 ByeMurof |
If this Information really helps, you could use the Rate function |
|
Follow us on