2/2/2022 6:22 AM | |
Joined: 8/30/2014 Last visit: 6/9/2024 Posts: 3 Rating: (0) |
Hi all, My problem is that when i disable the safety mode in tia portal 15.1 and make changes in safety FC i do not want that the PLC 1517F to go in stop. the question is why is going to stop the PLC 1517F if the safety mode is disabled? Thanks and regards El samad ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/02/2022 10:29:26New subject after splitting |
|
2/2/2022 10:45 AM | |
Joined: 9/21/2012 Last visit: 9/12/2024 Posts: 4131 Rating: (463) |
If a PLC is placed in to STOP, you can see the reason for that event, in the diagnostics buffer. |
Follow us on