(1)| 2/4/2022 3:23 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello dox365; The information and downloads from this document might be helpful: "Important! To use DIGSI 4 V4.94 Service Pack 1 on a PC with Windows 10 .Net Framework V3.5 must be installed manually. A respective message during the installation of DIGSI 4 like in older version is not displayed with DIGSI 4 V4.94 Service Pack 1. If .Net Framework V3.5 is not installed on the PC IEC 61850 devices can not be opened. Please do install .Net Framework V3.5 manually to open IEC 61850 devices again." Please check this webpage and see if this can solve your issues: https://support.industry.siemens.com/cs/pe/en/view/109740982 Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
Follow us on