2/8/2022 2:56 PM | |
Joined: 12/18/2014 Last visit: 10/5/2024 Posts: 33881 Rating: (4214)
|
SSA-316383: NumberJack Vulnerability in LOGO! CMR and SIMATIC RTU 3000 devices SUMMARY: A vulnerability has been identified in the underlying TCP/IP stack of LOGO! CMR and SIMATIC RTU
3000 devices. It could allow an attacker with network access to the LAN interface of an affected device to
hijack an ongoing connection or spoof a new one. The WAN interface, however, is not affected.
Siemens has released updates for the affected products and recommends to update to the latest versions |
Follow us on