2/8/2022 4:46 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
Yes, it's the actually LOGO! 8.3. In attachment you can see the article numbers of the expansion modules that you can use by the current LOGO!.
For the communication and program transfer you need only a simple ethernet cable.
For communication or program transfer you need necessary the current version LSC V8.3. You can download the free upgrade to LSC V8.3 from here: Download for LOGO! 8.3 Software UpgradeBut the download is export restricted and you need a extended registration: Why do you have to log in and register for downloading export-restricted software and what data do you need for this?AttachmentLOGO! 8 manual 0BA8 2021_05 xxxx8-0BA1 page 372.pdf (458 Downloads) |
Follow us on